Looking for ESD sensitivity data for the ADS7881IPFB. can't locate it on the web.
thanks,
Michelle
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Looking for ESD sensitivity data for the ADS7881IPFB. can't locate it on the web.
thanks,
Michelle
Hi Michelle,
The ADS7881IPFB passed ESD qualifications for three different test conditions/models:
ESD Test Models | Readpoints |
100pF, 1500 Ohms | 4000 V |
200pF, 0 Ohms | 200 V |
CDM |
1500 |
These models are representative of the Human-Body Model (HBM), Mechanical Model (MM), and Charged-Device Model (CDM). If you would like more information about these models check out the app note at: http://focus.ti.com/lit/an/ssya010/ssya010.pdf.
Best regards,
Chris