Part Number: ADS1278-SP
We have a power-up situation where the IO signals will temporarily turn on for appx 2ms when the DVDD/IOVDD/AVDD are not up yet. Each IO signal is limited to less than 0.5mA current during the 2ms start up period. unfortunately, this will likely turn on the ESD protection diodes on the IO lines which is not ideal. We're trying to assess the risk of part damage under such condition.
Do we know the maximum allowable ESD diode protection current limit for such a short period of time? What is the total amount of energy observed in your ESD test? thanks.