Part Number: ADC3662
Dear all,
We are designing a board with the ADC3662 configured to use the internal DDC feature with complex decimation.
We are wondering what will happen in case of an overflow?
We do not see any dedicated pin or status bit to get this information and the datasheet doesn't clarify this.
Will the output of the DDC saturate to maximum/minimum to indicate an input overflow?
In case this information is not available when using the internal DDC, disabling it will make it available in some way?
Thanks and best regards
Antonio Climaco