Hi expert,
If TX is only going to use as BPSK mode, should the DAC settings for DB0~DB13 all be set to 0?
Are there any other settings I need to be aware of?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi expert,
If TX is only going to use as BPSK mode, should the DAC settings for DB0~DB13 all be set to 0?
Are there any other settings I need to be aware of?
Thanks.
Hi Amy,
My customer is planning to mix the DAC output with an I/Q modulator.
Are you saying that if I use BPSK code for my DA[13:0], and set DB[13:0] all to 0 , it will operate BPSK modulation correctly?
Thanks.
Hello,
The setup can support BPSK, but we do not provide the tools to generate BPSK waveform.
Regards, Amy