Hi Team,
I have some enquiry on SCLK for ADS127L01EVM
1. Based on the section 8.5.2.2.2 (in data sheet), the setting of SCLK (the clock for SPI) should be any of-two ration of CLK cycles. So, is this means that for the CLK = 16MHz, the SCLK should be 16M Hz, 8M Hz, 4Mhz, or etc?
2. Would it be any data loss issue if 12Mhz SCLK is used for CLK = 16MHz?
Thanks!
Best Regards,
Ernest