This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8166: SPI-00 early data launch

Part Number: ADS8166

Hello,

The td_CKDO of the ADS8166 (19ns maximum) is not compatible with our master SPI that specifies a MISO Data Hold after SCK Rise of 40ns minimum.

Is there a configuration that can remove the early data launch of the ADS8166 SDO?

Thank you

Best regards

  • Hello Francois,

    Unfortunately, there is no way to disable the early data launch.  If your processor is fast enough for your desired data rate, you should be able to bit-bang the interface to ensure all timing requirements are met.

    Regards,
    Keith Nicholas
    Precision ADC Applications