Part Number: ADS1284
Hi to all users!
I'm planning to design ADC for seismic purposes.
Taking a look to ADS1284 datasheet I can see I can power ADS1284 with dual supply +/-2.5V.
Datasheet:
AVSS = from -2.6 to 0.0 [Volt]
AVDD = from AVSS+4.75 to AVSS+5.25 [Volt]
AINP or AINN = from AVSS+ 0.7 to AVDD– 1.25 [Volt]
If I choose AVSS = -2.5V, AVDD = +2.5V, I get AINP or AINN from -1.8 to 1.0 Volt, is this correct?
In this case I have these two options:
1) single ended, bipolar input signal
AINN to AVSS, AINP = from -1.0 to +1.0 Volt (so Vin = AINP-AINN = from -1.0 to +1.0 = 2Vpeak-to-peak)
2) differential bipolar input signal
AINN and AINP = from -1.0 to +1.0 Volt (so Vin = AINP-AINN = from -2.0 to +2.0 = 4Vpeak-to-peak)
Working with dual power supply I supposed negative range mirrired to positive range to cover full range....
Thanks.