This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC08100: How to reduce the power consuming

Part Number: ADC08100


We want to reduce the power consumption of the ADC08100.   Is the ADC08100 powered with 2.5 V a little less power consumption than the ADC08100 powered with 3 V?

  • Hi Enhui,

    The supply voltage is rated in the range of +2.7V to +3.6V, so TI cannot guarantee device performance outside that range.

    Power consumption is influenced by a number of settings, such as across sample rate (see Figure 25). Page 7 shows the power consumption under a number of test conditions.

    TI can only guarantee the power consumption to be the validated values listed in the datasheet.

    Regards, Amy