Hi,
ADC is in a serial mode by setting RST pin high.
To initialize the ADC registers via SPI port according to the data sheet bit 4 in ADC register at address 0x00 has to be set to 1.
Question:
Can we write our configuration to other bits of register 0x00 in the same SPI cycle (16 clocks) or
do we have to set D4 first in one SPI cycle and then write our configuration to register 0x00 in another SPI cycle?
Basically can you perform a RESET and configure register 0x00 within the same SPI cycle?
Thanks
Zlatko Pikal