Part Number: AFE5801
Hi Team,
A 200-kHz, 200-mVpp square wave generated by the signal generator couples a sine wave of the same frequency into the waveform output from the AFE5801. The customer would like to know how to remove this sine wave?
The signal takes a single-ended input and is AC coupled into the 5801 with a sampling rate set to 50 MHz. The waveform being picked at SignalTap is shown in the following figure, with the signal on channel one and channel two:

The output is set to unipolar output with register address 0x04[3] of 1. The customer has tried an LVDS test and receives a ramp output with register 2[15:13] of 111. Low-noise mode is enabled and register 7[10] is 1.
Could you help check this case? Thanks.
Best Regards,
Cherry