Hello,
I had some questions on the DAC121S101QML-SP Gain Error.
Do you have any estimate of the error of the DAC121S101QML-SP Gain Error at End of Life (aka ageing effects, is it an extra +/- 0.1%FSR over life, +/- 1%FSR over life, etc).
Also, the gain error over temperature is +/- 1%FSR over temperature but that is for VA 2.7V to 5.5V (see Table 6.5 below). Is it better at VA = 5.5V, Figure 23 seems to imply that (also shown below) but the table is all-inclusive and doesn’t specify a difference at various VA values.
Thanks,
Adam