This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1601, 3.3V nominal DVDD instead of 3V?

Other Parts Discussed in Thread: ADS1601

The ADS1601 seems to want DVDD = 3.0 V nominal. It has a range of 2.7 – 3.3 V, and is tested at 3.0 V.

 Is it OK to have DVDD = 3.3 V nominal? (+/- 3% I suppose, which would make it 3.4 V max)

 I can put in a 3V regulator, but I am using 3.3V for other logic and stuff.