In SBAA180 document(example temperature measurement applications using the ADS1247 and ADS1248),
page 6, second content,
Why is the maximum differential input to the modulator is equal to [(AVDD-AVSS)/2] ???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Chang Yu Cheng,
Welcome to the forum! 2.5V is the desired reference voltage created with 3mA going through the Rbias resistor (833.3 ohms). This reference voltage value is the maximum allowable +/- swing for AVDD-AVSS=5V. This is also assuming a PGA gain of 1.
Later in the text the example refers to PGA=128, which will reduce the input range to +/-19.5mV.
Best regards,
Bob B