Other Parts Discussed in Thread: ADS1299
Hi TI Teams,
Our of our customer reported that the operating current was much higher than the datasheet current when they tested the power consumption of ADS1299-4. When all 4 channels are turned on the operating current is about 10mA (with the analog power supply is 5V and digital power supply is 3.3V) , while the datasheet has a current value of only about 5mA.

The operating current with all channels closed is about 2.5mA,each channel opened will increases the operating current by about 2mA, and the number of channels turned on increases the current by 2mA in equal proportions. They also do a lot of experiments but don't see any improvement in this operating current.
The schematic is as below:

The register setting as below:

Can you help to analyse the cause of the problem? Or can you give us some suggestion for this?
Thanks,
Kind Regards