Does the ADC support DES mode with 1:4 Demux and SDR? Basically, we are looking to use the mode in Figure 6 but with SDR instead of DDR. Table 10 does not mention 1:4 Demux mode so it isn't clear if that is supported with SDR.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does the ADC support DES mode with 1:4 Demux and SDR? Basically, we are looking to use the mode in Figure 6 but with SDR instead of DDR. Table 10 does not mention 1:4 Demux mode so it isn't clear if that is supported with SDR.
Hi Cris,
I am checking on this and will get back to you next week.
Thanks,
Amy
Hi Cris,
The ADC12D1620QML datasheet details the modes that the device supports. The 1620 is just an increased speed grade version of the 1600. Table 7-8 in the 1620 datasheet lists out all the modes, including the DES mode with 1:4 Demux and SDR combination you are looking at. This will work in both LSPSM and Non-LSPSM modes.
I can test this for you in the lab, if you would like confirmation that this is indeed true for the 1600.
Regards, Amy