Hi,
I have been watching the video series and have a question on the SAR reference input model video.
From this video I have developed a model for the F28388D MCU but am uncertain on the results.
A screen shot of the video is shown below. It indicates that if the error reads 0 then everything is fine.
When I run the simulation VrefError corresponds to Vref error. I can see Vref charging when the switch is closed but it does not charge all the way to its final value. When the switch is open Vref jumps up to it expected value so its error is near zero like the video indicates. However the voltage sampled on the node Cref in the slide (VchError below) is -80 mV below expected value. The video does not say anything about what Cref should be at just Vref. Will the measurement have -80 mV of error?
Thanks,
Jennifer