Hi:
Page 25 has a paragraph that talks about not driving the analog/digital inputs prior to applying the supply voltages:
"The analog and digital supplies should be applied
before any analog or digital input is driven. The power
supplies may be sequenced in any order. The internal
master reset signal is generated from the analog
power supply (AVDD – AVSS), when the level
reaches approximately 3.2 V. The power-up master
reset signal is functionally the same as the Reset
Command and the RESET input pin."
We are using the ADS1258-EP ADC in one of our recent designs and would like to understand this some more.
Why is it is required that the supply voltages are applied first? We think is to avoid damaging the ESD diodes.
If that is not the reason, then why is it? and what is the potential damage that can occur?
In our design we are Is there a voltage range (or a current range) on the analog inputs that it can tolerate without no damage?
Thanks