Other Parts Discussed in Thread: TX7316
Hi,
1. Should SEN be held low between the two SPI cycles required for the read operation?
i.e Will two normal SPI reads with SEN going high between the cycles not work?
Please clarify.
2. Is there any special setting for SPI read with a single cycle as in TX7316?
3. Is it OK to discuss here?
Ravi Ganesh