This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC53202: Can't readback any registers via SPI

Part Number: DAC53202


Hi,

    I‘am using DAC53202,the output current and voltage of the DAC can be correctly changed by configuring the DAC-X-DATA, but when trying to read back any register, the SDO pin is always at the IO level.

    The clock cycle of the read back is 1.27us.

    I suspect that the GPIO is not properly configured as SDO, so I tried many different combinations of the relevant configurations in the registers such as  COMMON-TRIGGER, COMMON-CONFIG, INTERFACE-CONFIG, GPIO-CONFIG, etc., But it never changed the situation that the SDO was always high.

    Can you provide a correct copy of the readback sample code? Or have any cases of successful readback to share?

Best reguards!

vr