Other Parts Discussed in Thread: DAC8771, DAC8760, DAC63202
Hi,
Is it possible to use the DAC8771EVM as a 1KHz arbitrary waveform generator? The datasheet does not specify maximum sample rate. Thus, I presume it is only meant for static operation.
But I am looking for a DAC that support negative to positive outputs (approx +/-5V output). The DAC8771 fulfills the pos/neg output voltage well. But can it be used to generate arbitrary waveforms?
The SPI-Interface makes this a little difficult because it has write overhead. And driving it with a real-time OS computer (Raspberry Pi) does not make it easy to control an equal spaced sampling rate.
My main questions:
1. Is it possible to use the DAC8771EVM for the above mentioned application? (1KHz AWG +/-5V)
2. If there is another part that is more suited for this application, could you please suggest one?
Thanks,
Steven