Other Parts Discussed in Thread: OPA862, ADS1120, ADS112C04
This is my setup for bi-directional measurement of DC battery cell voltages battery set voltages ranging from 0.1V to 600V using ADS1115 (changing gain with help of PGA feature) with ATMEGA328 programmed by Arduino. This circuit is working well with good accuracy but, I want to put a differential amplifier (or) voltage buffer circuit at the input stage of ADS1115 to increase it's input impedence.. plz suggest me suitable differential amplifier IC model(s) or precesion op amps for making voltage buffers to drive the ADS1115 inputs. Thanks in advance!!!