In section 3.9 of the documentation, "Open the TSW12QJ1600EVM GUI and Program the ADC and Clocks", figure 3-2 shows a GUI called "ADC12QJxx00 TI Design GUI". The only program listed in the support software section for this part is called "SLAC809". However, it is a completely different program which, when installed, doesn't have the same name or show any of the panels that are shown in the documentation. It seems to be some kind of TCP interface. I think someone mixed up the programs that are available.