This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC63004: Daisy-chain operation without NVM

Part Number: DAC63004


Hi,

I'm trying to configure daisy-chain operation, as detailed in the datasheet.

First thing is to set SDO-EN in the INTERFACE-CONFIG.  This should cause SDO (the GPIO pin) to output the end of the shift-register.

But I think there is a bug because although SDO does reflect the output of the shift-register for bits [22:0], bit 23 is always asserted.

This is the 'read/write' bit, now set to 'read', so you CANNOT write data to the next devices in a daisy-chain.

Has anyone else come across this?

Have I found an un-fixable bug?