The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4249EVM: Large HD2 on ADS4249 EVM

Part Number: ADS4249EVM

Dear TI-

I am working with the ADS4249EVM and TWS1400. Both of these are in the stock/out-of-the-box configuration. I am observing larger than expected spurious in the FFT. Additionally, the codes view appears to have a pronounced AM envelope. I have attached a couple images from a specific scenario with the following setup;

100MSPS, +20 dBm+LPFx2

SOI 65 MHz, +20 dBm+10 dB pad +LPF+BPF

As you will see HD2 is ~43 dBc at 5 MHz. The AM envelope is also 5 MHz. We believe our clock and SOI sources (all 50-ohm) to be clean. HD3 appears close to datasheet level. Is it possible this is a result of mismatch in transformer parasitics? If I change sampling rate and SOI frequency, etc., I am still largely spur limited. Any insight is greatly appreciated