This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggest the suitable products which will fulfill our application

Other Parts Discussed in Thread: ADS1220, ADS124S06, ADS122U04

Dear sir,

we have requirement of one MCU , 24-bit ADC  and processor Board, I will explain our application, The 12 channel RTD system is used to read the data from 12  temperature sensors(4-wire RTD) with channel to channel isolated ADC Board we required. in our case 12 channel is not available in single board we will use 2 or 3 boards. Each channel can accept either a thermocouple or a RTD input. our application consists  of 3 parts 

1) ADC module : to read the 4-wire RTD sensor data

2) Microcontroller :ADC connected to this microcontroller and having the external SD card support to store the ADC data 

3) Processor Board: to control the total operations using GUI which is running in the Processor.

External ADC having the below specifications:

1) DC Resolution: 24 bits or higher

2) sampling rate : minimum 5 samples per second for each channel

3) PT-100 3 wire/4 wire RTD we will use.

4) channel -channel isolate ADC board.

Microcontroller having the below specifications

1) ARM-cortex-M3 processor

2) 32 bit data  bus width

3)Ethernet support-1 or more

4) 2 channel ADC >=12 bit resolution to read the pressure sensor data.

5) Serial RS-232 support

Microprocessor consists of the below following specifications


1) Microprocessor:Cortex-A57 or A72, 64 bit High speed, multicore processor


2) Operating system: Real time Linux Better for running embedded applications


3) Base Clock Speed of Processor >=1.5 GHz


4) No. of Cores:4 (Quad)


5) RAM Size: 4GB or better


6) GUI QT based


7) LCD 7-inch LCD display support


8) Mouse and Keypad support

9) External SD card support to store the ADC data

please suggest the 3 things ADC, controller , processor board which can fulfill our requirement form your products list.

Thanking you...!

Best Regards

Raj