Part Number: ADC08100
Hello. I am currently testing a design using your ADC08100 converter. The ADC data is processed by an FPGA, that takes sums 24576 consecutive windows of 3072 samples.
I am, however, experiencing an unusual noise on the data, and would like to understand why. The schematic is the following.

As said before, we have a program that takes 3072 samples from the ADC and stores it in memory. It does 24576 accumulating the data.
The ladder reference voltages are set up from 1.48V to 0V.
The ADC was connected through a short 50-ohm coaxial cable to a waveform generator and properly terminated. Here are some of the results.
Stable when input is 0V.

High synchronous noise when input is 0.5 V


A more random looking noise when input is 0.75 V. This is what I would expect for all tests. The amplitude of the noise is much lower too.


Stable when input is 1.5 V.

One period (0-1V) 100 kHz sine wave, triggered by a pin on the FPGA, synchronously (but with a delay) with the beggining of the sampling window. High synchronous noise when signal is DC.



Could this be an issue with my implementation of the ADC08100, or could it be an issue in the processing system? I think that the FPGA is executing correctly because the results are repeatable and seem correct.
NOTE: The issue still happens when the clock frequency is decreased to 50 MHz