This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3683: FCLK duty cycle is abnormal

Part Number: ADC3683


Hello,

One customer used ADS3683 and wanted to configure the Decimation Bypass, 1-wire, 16bit mode, below is the configuration, but the FCLK duty cycle is not 50%.

I found the 0x20~x022 has no problem and 0x1B =0x88, I wonder why the FCLK is abnormal. Please help to analyze:

// 011 0 1 100 -- 0x6c -- 1-wire
write_reg(fd, 0x07, 0x6c);
printf("reg 0x%02x = 0x%02x\n", 0x07, read_reg(fd, 0x07));

// load e-fuse
write_reg(fd, 0x13, 0x01);
usleep(2000);
write_reg(fd, 0x13, 0x00);
usleep(2000);

// configure FCLK
// Decimation Bypass
// 0 00 0 000 0
write_reg(fd, 0x19, 0x00);
printf("reg 0x%02x = 0x%02x\n", 0x19, read_reg(fd, 0x19));

// Decimation Bypass
// 1 0 001 000 -- 0x88, 16bit
write_reg(fd, 0x1B, 0x88);
printf("reg 0x%02x = 0x%02x\n", 0x1B, read_reg(fd, 0x1B));

// FCLK
// 0x0FF000, 16bit
write_reg(fd, 0x22, 0x0F);
write_reg(fd, 0x21, 0xF0);
write_reg(fd, 0x20, 0x00);

printf("reg 0x%02x%02x%02x = 0x%02x%02x%02x\n", 0x22, 0x21, 0x20, read_reg(fd, 0x22), read_reg(fd, 0x21), read_reg(fd, 0x20));


write_reg(fd, 0x24, 0x00);
printf("reg 0x%02x = 0x%02x\n", 0x24, read_reg(fd, 0x24));

write_reg(fd, 0x25, 0x00);
printf("reg 0x%02x = 0x%02x\n", 0x25, read_reg(fd, 0x25));

The readback value is

And the FCLK curve is as this:

Best regards

Kailyn