This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32RF45EVM: Capture large amounts of raw data with HSDC Pro GUI 6.0 and TSW14J56EVM

Part Number: ADC32RF45EVM


Hi

I am using a TSW14J56EVM with ADC32RF45EVM and HSDC Pro GUI 6.0 version. I am not able to capture larger raw data files with this setup ( which I was able to do in earlier versions of HSDC Pro GUI 5.1 and 5.2). I was earlier able to capture data up to the max limit of 4GB (1GS/channel * 2bytes/channel * 2 channels). Do I have to install something extra to make it work with the new version of HSDC Pro GUI 6.0? Also, I am using a brandnew PC running Win 11 to get this data capture. Attached is a screen shot of the error I obtain when I try to get 8388608 samples per channel.  Do you have any leads to circumvent this error? Also, Is there a way for me to get the earlier versions of the HSDC Pro GUI say 5.1 or 5.2 ?

  • Hi Aravind,

    We have recently noticed that some machines are not installing version 6.0 correctly which may be the sole cause of all your issues. We are looking into the issue but are unsure of a timeline. In the meantime, please use version 5.2 as requested which is available from the link below:

    TI Drive: https://tidrive.ext.ti.com/u/_c00lcVNNNHvzTSS/2f3bd4de-1827-4da1-a0b7-805d75cb10c6?

    Access Code: UfD9Q?6J

    Thanks, Chase