This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8686S: Byte Parallel communication issue with ADS8686S

Part Number: ADS8686S

It has relationship with this issue: https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1309747/tms320f28388d-emif-configuration-of-the-oe-wen-cs

I want to ask you, on basis what I wrote in that thread, what would happen in the Byte Parallel communication with the ADC if I want to read a Channel A conversion if I put up the CS after the first 8 bit reading and then pulling it down. I will show you in the picture:

It would be a problem if any time I finish a 8-bit reading (RD high) I deactivate the CS and then put them low to read the next 8-bit reading of the same conversion result?

The same I would like to ask you with the writing register:

I could put up the Chip Select between the two 8-bit frames of a complete 16-bit frame??