This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS127L11: SPI from ADS127L11 to ST32. Can the 24-bit SPI frame be received by H743ST32

Part Number: ADS127L11

Can ADS127L11 send 32-bit samples in 2 or 3 SPI frames?

We are trying to use ADS127L11 with all 24-bits. and to send the samples to the H743ST32.

The datasheet for the microcontroller mentions the 8 and 16-bit SPI frames, but not 24-bits SPI frames.

Is it possible to send the 24-bits ADC samples through 2, or 3 SPI frames instead of one?

I will much appreciate anu help or insight about this, as well as direction to the related forums and answers that are closely related to this question.

Regards.

Vlad Pavlovic