Part Number: ADS130E08
I'm a little confused by the stated analog input range and diagram when ADS130E08 is configured for single-ended input. Figure 18 shows the input range as CM voltage (INN) +/- Vref/2.

Ignoring CM range concerns and assuming Gain = 1, why is this limited to Vref/2? The ADC code range goes from -Vref to +Vref so it seems the input range can be larger than Vref/2.
The reason for this question is if the INN inputs are tied to a voltage closer to a one of the supply rails rather than mid-range, it will obviously limit the ADC range in one direction as the input gets approaches the closer power rail, but what about the other direction where there is more margin to the power supply, is the input really limited to Vref/2 in this direction?
Taking this to an extreme, if INN is tied to AVDD, the positive half of the ADC range is not available as this is above AVDD, Is the lower half of the ADC range reach all the way to -Vref or Vref/2? I understand that inputs within 0.2V of AVDD are not valid as this violates the PGA CM range.