This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3563: External reference for 1.6V

Part Number: ADC3563
Other Parts Discussed in Thread: ADC3644, ADS8860

Dear Technical Support Team,

According to "8.3.3.2 External voltage reference (VREF)", it is required 1.6V for  VREF.

Could you please provide information on the recommended circuit for the reference voltage?

For example, REF35160 is 1.6V reference voltage IC.

Is it possible to connect REF35160 and VREF of ADC3563?

REF35160 seems not to integrated ADC Drive Buffer, so external opeamp is necessary(REF35160 ⇒OPA⇒VREFof ADC3563)? 

Best Regards,

ttd