This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8557: operating mode without HVDD/HVSS voltages

Part Number: ADS8557

Hello,

Question related to ADS8557IPM: If we have no HVDD/HVSS voltages (due to a failure in a DC/DC converter for example). Would the digital part still work? I mean, if we have HVDD=HVSS=0V; and AVDD=BVDD=5V, would BUSY signal go up and down (we assume that the converted values woud have nos sense)? Or it would stay always down? (we have CR bit 21='0').

In this situation, what would be the expected read value? All '0's or full-scale value?

Thanks,