Hi,
Does DAC39RF10 have timing delay function?
For example, when it works under 3GSPS, can it delay output as few sampling clock?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Does DAC39RF10 have timing delay function?
For example, when it works under 3GSPS, can it delay output as few sampling clock?
Thanks.
Hey David,
As the DAC uses a serial JESD204B interface the latency is quite variable across different input modes. In addition things like interpolation add additional latency. There are ways to make this latency deterministic in a given mode of operation but the overall latency of the DAC is not well defined.
Regards,
Matt
Hi Kramer,
You mean that JESD204B and interpolation can make latency but DAC can't control this latency with some register setting.
Is it correct?
Thanks.
Hey David,
That is correct. The latency of this device can be impacted by several factors; but there is not a simple way to add N clock cycles of latency with a register write.
Regards,
Matt