Hello team,
On the datasheet, there are DAC-0 and DAC-1.
Are they meaning DAC-0 = OUT0 and DAC-1 = OUT1?
If so, DAC63001 has only OUT0, so I can ignore DAC-1?
Best Regards,
Kei Kuwahara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
On the datasheet, there are DAC-0 and DAC-1.
Are they meaning DAC-0 = OUT0 and DAC-1 = OUT1?
If so, DAC63001 has only OUT0, so I can ignore DAC-1?
Best Regards,
Kei Kuwahara
Hello,
Yes, this datasheet is shared between the single and dual channel device. If you are using the single channel device (DAC63001) you can ignore OUT1. The registers for OUT1 will not have any effect on the DAC63001.
Best,
Katlynne Jones