Hi,
Would it be possible for someone to review my ADC error calculations? If so, what would be the best way to share that? I'm seeing that errors on the order of 0.5mV are causing errors in the corresponding temperature reading of 0.35C at 125C (using an 0.01%, 5ppm/C bias resistor). It seems like a rather large error so I just would like to see if I'm handling the sensitivity analysis correctly.
Thanks,
Drew