Hi expert,
Can you help elaborate why the maximum output is derived as below?
Per our understanding, it should be derived as this equation.
Thanks,
Zach
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zach,
I agree with you that the maximum output should be calculated by (VFB*2) - DACmin so that the differential between the margin high and margin low values are equal (if the goal is to margin by +/- a certain percentage). The equation you underlined works out when VFB is 0.6V, but not for other values. I'm not exactly sure where it was derived from. I would just recommend that you keep the maximum code at least 1% below the DAC full-scale code to avoid any error from the DAC full scale error.
Best,
Katlynne Jones