Part Number: DAC11001B
Is there a time diagram for the generation of continuous signals where SYNC is always low and the values are loaded exclusively via Load? There is no timing for the the delay from the shift register input to output and there is no timing for the set-up time of the 32 bit storage register.
In other words if the last bit of 32 bits is entered into the shift register with the falling edge of the clock what is the minimum delay between falling edge of the shift clock and the falling edge of /load signal?