This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC53204: VOLTAGE LEVEL TRANSLATION

Part Number: DAC53204
Other Parts Discussed in Thread: TCA39306, PCA9306,

Hi,

To perform voltage margining through DAC53204RTER. We have used MUX with I/O voltage of 1.8V to drive the I2C lines of DAC. DAC's I/O voltage is 5V.

We are planning to use I2C level shifter with smaller footprint/package. We found the parts TCA39306 and PCA9306.

Please let us know which level shifter can be used from the above two parts.

Also attaching the design for your reference.

  

Thanks

S Sathya shree