Assuming a condition where the ADS1258-EP is unpowered on the digital & analog supply voltages: the Abs Max datasheet lists 10mA continuous (to protect ESD diodes).
1) Is that 10mA max the limit for each of the Analog & Digital Inputs? Or is it a 10mA max limit for all inputs on the whole package?
2) Page 42 has recommended input protection – however the leakage on the diodes can impact the analog signal & accuracy and for this reason they want to be avoided. Would just a limiting resistor be sufficient protection during an unpowered event?
3) 10mA is the abs max continuous limit - as stated in datasheet you would never want to operate this high - and obviously lower is better. Are there any suggestions at a reasonably safe current limit to meet on the inputs of this ADC during an unpowered event. Not looking for any sort of binding recommendation from TI, but a ballpark number that a designer could feel good about... if they had to design for an unpowered event with voltage on the inputs - any insights here are appreciated.
4) Page 25 - are there any sequencing requirements between the analog supply voltage and digital supply voltages? (Digital last on, first off?)
Thanks,
-Chris