This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS112C04: Could ADS112C04 be used in two channel RTDs applications?

Part Number: ADS112C04
Other Parts Discussed in Thread: ADS1147

Hi team,

We have a question about the ADS112C04:

Could ADS112C04 be used for two channels RTDs.

In the datasheet, the typical application is just for 1 channel RTD.

If we want to use 1 chip to test 2 channel RTD, the sampling rate may not higher than 20 sps (means that we will test 2 channel data in 50ms).

Our thought is we use the AIN0 & AIN1 test 1 channel RTD, and AIN2 &AIN3 test another channel RTD, the 2 channel RTD share one Rref,  but sample in different time.

 It works in ADS1147, please help to confirm whether it also works in ASD112C04. The external connection with the RTD and pins are following:

Best Regards,

Matt.