This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80504: Can the internal reference output be used externally to provide reference voltage to the external ICs?

Part Number: DAC80504


Hello,

The datasheet of DAC80504 says +/-5mA(typ) for the reference load current on page 9 in the datasheet, but can it be used externally to provide the reference voltage to the other external ICs if it has enough current margin?  Or is it dedicated for internal use only even though it has a little capability of load current?

Best Regards,

Yoshikazu Kawasaki