This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC53701-Q1: What is the variation of the internal reference?

Part Number: DAC53701-Q1

Hi,

We are using DAC53701-Q1 in a design and we need to calculate the accuracy of our full design. We use the internal reference voltage but I can not find a spec for the min and max values of the reference voltage (only typical 1.212V) and the gain. I would also like to know the variation on the reference voltage gain under temperature.

Kind regards,

Louis