Hello,
I want to develop a compact digital readout circuit for two DDC2256A devices.
I've already inspected the DDC2256EVM and designed an analog circuit with our sensors and two DDC2256A devices which can be read out using the digital board of the EVM and the TI DDC2256_EVM_GUI software.
In the next step I want to develop my own digital readout-circuit for my analog board.
Since I'm a physicist and yet have never touched FPGA-programming, my first question is, whether it is possible to controll the two DDC2256A devices using a microcontroller and if so, can you recommend a suitable device?
In case it is not possible to use a microcontroller, can you provide a minimum FPGA-based design approach?
My ultimate goal would a compact USB-powered handheld device for our sensors based on two DDC2256As.
Many thanks in advance for your advice!
Best regards
Alexander