Part Number: ADS7953
I have ADS7953 and ref4132-3.0v.
The power supply voltage of my system is 5V and the reference voltage is 3.0V.
If the ADC input signal is 4.0 Vpp,
I have problems for these 2 cases
1) 1xVref
Does digital output is full scale 0xFFF?
2) 2xRef
Does digital output is 0xAAA (2730/4095)?
For the case 2, if my input voltage doesn't exceed Vs(5.0V), then it can't damage ADC, right?
Best Regards!
De Wei