This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7128: Need the programming steps to set up and capture an ADC sample on the ADS7128.

Part Number: ADS7128


I have the exact same question as  posted 11months ago, and there is no posted answer in the Forum.

Need the programming steps to set up and capture an ADC sample on the ADS7128.

I have 0.5V on CH_0 with a 3.3V reference. Just want to capture the 12bit ADC conversion via I2C

I can read and write to all registers on the part, but am unsure of the call sequence to set up and capture the data.

The Spec is vague

Any help is appreciated.

-t