Part Number: ADS7828
What is the max. voltage range for the analog input channels ? is it 0V to Vdd + 0.2V ? OR 0V to Vref (2.5V) ?
The part # is ADS7828EB
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS7828
What is the max. voltage range for the analog input channels ? is it 0V to Vdd + 0.2V ? OR 0V to Vref (2.5V) ?
The part # is ADS7828EB
Hi Benny,
The Full Scale input range of the ADS7828 is 0 to Vref. If you are using the internal reference, that would limit you to 2.5V. The ABS MAX input range (before potential damage to the part) is -200mV to Vdd + 200mV.