The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1261EVM: Enabling PGA introduces a scale factor affecting voltage readings

Part Number: ADS1261EVM
Other Parts Discussed in Thread: ADS1261

Hi I have an issue with ADS1261 eval baord. Whenever the PGA is enabled the values read by the ADC are scaled, and dont match their true ampltude. When the PGA is bypassed the ADC reads acceptable values. What would be the cause of this?

I confirmed the input voltage of the ADC with 2 keithley multimeters connected in parallel. I have tested without multimeters and still get the same result. Here are plots from my test. I have also placed the EVM board in an insulated case with a heating pcb attached to the ADC chip with thermal paste. The temp of the ADC was stabilized to 55C according the internal temp sensor. This was done to ensure ambient temperature isnt affecting the readings.

PGA enabled gain 1

PGA enabled gain 128

PGA bypassed (I used smaller voltage steps for this test but its clear the scale factor is much less compared to PGA enabled)

Here is the configuration of the register as im using the TI ADC software to read values

PTC ADC device file.txt
[ADS1261 Register Settings]
ID             	80
STATUS         	01
MODE0          	04
MODE1          	01
MODE2          	00
MODE3          	00
REF            	15
OFCAL0         	00
OFCAL1         	00
OFCAL2         	00
FSCAL0         	00
FSCAL1         	00
FSCAL2         	40
IMUX           	FF
IMAG           	00
RESERVED       	00
PGA            	80
INPMUX         	34
INPBIAS        	00

I'm posting here as a last resort to figure out why this issue is happening thanks for reading! Let me know if i missed any details and will fix that right away.

  • Hi Atlin Anderson,

    This appears to be some sort of gain error. You can see that as the input signal increases, so does the variation. If plotted this error, it would probably look pretty linear.

    You should try calibrating the ADC and see if that improves the situation

    -Bryan