This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC2574 unstable

Other Parts Discussed in Thread: TLC2574

We have a new design using the TLC2574 in single ended mode. We use as reference voltage the ADR434AR with adjustable output, set to 4.0V. We connected several external sources and noticed that the readings are not stable. We even connected the reference voltage (4.0V) as one of the inputs just to test the stability. We read the ADC once a second and get readings changing in the range of 2850 to 2870. We expected changes of 1 LSB (+/- 5 mV) but not that much (equivalent to almost 100 mV). What can be the reason of that unstableness?

Thank you for your help