Tool/software:
The reference voltage for ADS7924 is writen “Supply” on the TI web and the datasheet. Does the device generate a reference voltage internally from the voltage of AVDD pin? Does the ADI scale remains constant no matter how many volts I apply to AVDD within the recommended operating voltage range? As a specific example, if 2.2V is applied to ADI CH1, will the converted and output digital value be the same even if AVDD fluctuates in the range of 5.5V to 2.2V? For example, in the battery-powered case.